Expansion of the MEGAOHM™ range: the insulated bearing that protects electric motors
- France - Industry OEM - Products
The use of variable frequency drives on electric motors is the cause of numerous failures, linked to the flow of high-frequency currents inside the bearing. These eddy currents can cause premature damage to components and compromise the reliability of the equipment.
To address this issue, NTN has developed the MEGAOHMTM range, a range of insulated bearings designed to effectively protect electric motors against the effects of eddy currents.
A comprehensive and high-performance range

NTN is expanding its MEGAOHMTM range to meet an even wider range of requirements. This expansion involves the addition of bearings fitted with a sheet-metal cage, suitable for small motors. These complement the brass-cage version, which is intended for larger motors.
The MEGAOHMTM bearing offers, above all:
- High-performance electrical insulation thanks to a ceramic coating
- Electrical resistance of up to 3000 VDC
- Two ranges available depending on the application: sheet metal cage and brass cage
- Compatibility with standard bearings, facilitating integration
The availability of the MEGAOHMTM range
The availability of the range across all standard part numbers is a real advantage for coil winders and electric motor maintenance professionals, who often need to get hold of the right part quickly to ensure repairs are carried out as promptly as possible.
NTN Europe, partner of the Béjuit Racing Truck at the 24 Hours of Trucks
- France - Automotive Aftermarket - Events
On 26th and 27th September 2026, NTN Europe supported the Béjuit Racing Truck, the team from the Emile Béjuit vocational college, at the 24 Hours of Le Mans for Trucks on the iconic Le Mans circuit. Through this partnership, NTN Europe is supporting an educational project whilst showcasing… Read more
NTN Europe joins forces with OCP Maintenance Solutions to develop industrial predictive maintenance using AI
- France - Industry OEM - Events
On 21st September 2026, NTN Europe and OCP Maintenance Solutions, a deep-tech company specialising in predictive maintenance, announced a strategic partnership. The aim is to support European manufacturers in improving the reliability, availability and performance of… Read more