Presă

Mai jos veți găsi comunicatele și dosarele de presă ale NTN în Europa privind structura acesteia, produsele, serviciile, tehnologiile, inovațiile sale etc.

29 rezultat(e)X
ntn-snr-ensures-the-quality-of-its-customs-processes
Noiembrie 2016 - Companie

NTN-SNR ensures the quality of its customs processes

NTN-SNR acquired AEO (Authorised Economic Operator) status, as certified by the Léman Customs Directorate on 27 September 2016. This European certification consecrates NTNSNR's approach to...

Citiți comunicat de presă:
pressrelease
Noiembrie 2016 - Companie

NTN-SNR présente une offre globale du guidage linéaire au roulement pour toutes les chaines de packaging

NTN-SNR est présente pour la première fois au salon All for Pack à Paris du 14 au 17 novembre pour présenter son offre globale pour les chaines de packaging. Celle-ci se décline avec une gamme...

Citiți comunicat de presă:
pressrelease
Septembrie 2016 - Piețe

Press kit: Automechanika Frankfurt - From 13th to 17th September 2016

At the Automechanika 2016 trade fair, which will run from 13th to 17th September 2016 in Frankfurt, NTN-SNR is launching two new ranges: a range of constantvelocity (CV) joint kits intended for...

Citiți comunicat de presă:
pressrelease
Iulie 2016 - Companie

The NTN-SNR Polipump has a good track record with Véolia

Since its launch in 2012, the NTN-SNR Polipump has been a real success. This multipoint unit offers up to 35 lubricating points with a pressure of 80 bar per point and easy and efficient...

Citiți comunicat de presă:
pressrelease
Iulie 2016 - Piețe

NTN-SNR have developed a wireless position-measuring system for their linear modules

NTN-SNR have developed a linear module featuring a wireless position-measuring sensor built into the linear guidance system. Its compactness, ease of implementation and lack of wires make it a...

Citiți comunicat de presă:
pressrelease
Iunie 2016 - Piețe

NTN-SNR's wide product range, modularity and innovations cover all automated movement needs

For the first time, NTN-SNR shall take part in Automatica, the international trade fair for robotics, automation and mechatronics to be held from 21 to 24 June in Munich. NTN-SNR is a major player...

Citiți comunicat de presă:
pressrelease
Mai 2016 - Companie

NTN-SNR mobilized in the fight against forgery

NTN-SNR bearings are prone to copying or forgery. Increasingly sophisticated forgery techniques observed for several years make it virtually impossible for the untrained eye to distinguish non-...

Citiți comunicat de presă:
pressrelease
Aprilie 2016 - Companie

NTN-SNR Clean Sky bearings honoured by the European Union

NTN-SNR’s project to supply bearings for Snecma's Open-Rotor engine demonstrator was among the 10 projects of the European Clean Sky research programme to be shortlisted to receive one of three...

Citiți comunicat de presă:
pressrelease
Decembrie 2015 - Companie

Des médailles par centaines !

NTN-SNR ROULEMENTS, premier employeur privé des deux Savoie, a récompensé l’ancienneté et la qualité de ses salariés par la remise de Médailles d’Honneur du Travail.
275 distinctions au...

Citiți comunicat de presă:
pressrelease
Noiembrie 2015 - Companie

Procédure arbitrale initiée par un constructeur de poids lourds à l’encontre de NTN-SNR ROULEMENTS

En novembre 2012, une procédure arbitrale a été initiée par l’un de nos clients sur son propre territoire, pour des dommages allégués sur leurs moteurs,qui résulteraient du fonctionnement de...

Citiți comunicat de presă: