Mai jos veți găsi comunicatele și dosarele de presă ale NTN în Europa privind structura acesteia, produsele, serviciile, tehnologiile, inovațiile sale etc.
Presă

NTN-SNR ensures the quality of its customs processes
NTN-SNR acquired AEO (Authorised Economic Operator) status, as certified by the Léman Customs Directorate on 27 September 2016. This European certification consecrates NTNSNR's approach to...

NTN-SNR présente une offre globale du guidage linéaire au roulement pour toutes les chaines de packaging
NTN-SNR est présente pour la première fois au salon All for Pack à Paris du 14 au 17 novembre pour présenter son offre globale pour les chaines de packaging. Celle-ci se décline avec une gamme...

SNR Cévennes « Vitrine Industrie du Futur »
SNR Cévennes, filiale de NTN-SNR Group, est fière d’annoncer l’obtention du label « Vitrine Industrie du Futur » par son usine de Croupillac à Alès dans le Gard, qui produit des roulements de...

Press kit: Automechanika Frankfurt - From 13th to 17th September 2016
At the Automechanika 2016 trade fair, which will run from 13th to 17th September 2016 in Frankfurt, NTN-SNR is launching two new ranges: a range of constantvelocity (CV) joint kits intended for...

NTN-SNR innove : Des joints de transmission et des roulements de boîtes de vitesses seront lancés a Automechanika !
À l’occasion du salon Automechanika 2016 qui se tiendra du 13 au 17 septembre 2016 à Francfort, NTN-SNR lance deux nouvelles gammes : une gamme de kits de transmission destinés au parc européen et...

The NTN-SNR Polipump has a good track record with Véolia
Since its launch in 2012, the NTN-SNR Polipump has been a real success. This multipoint unit offers up to 35 lubricating points with a pressure of 80 bar per point and easy and efficient...

NTN-SNR have developed a wireless position-measuring system for their linear modules
NTN-SNR have developed a linear module featuring a wireless position-measuring sensor built into the linear guidance system. Its compactness, ease of implementation and lack of wires make it a...

NTN-SNR's wide product range, modularity and innovations cover all automated movement needs
For the first time, NTN-SNR shall take part in Automatica, the international trade fair for robotics, automation and mechatronics to be held from 21 to 24 June in Munich. NTN-SNR is a major player...

NTN-SNR deploys 2 flagship products for towed agricultural machines
After their launch at the end of last year, NTN-SNR is deploying its offering of built-in hubs and inserts for self-aligning bearing units for all manufacturers of agricultural machines and...